Part Number: ISO1212
AC入力の時、全波整流を行いISO1212に入力する電圧をDCに変換しているが、リップル(0V)の瞬間がうまれてしまうのではないでしょうか?例えば200Vの電圧がかかっているとき、理想はISO1212の出力がずっとONです。しかし、しきい値を下回りhigt/low繰り返すと考えられます。
教えて頂きたいです。よろしくお願いいたします。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When inputting AC, full-wave rectification is performed and the voltage input to ISO1212 is converted to DC. Isn't it possible that a ripple (0V) moment will occur? For example, when a voltage of 200V is applied, ideally the ISO1212 output is ON all the time. However, it is considered that it repeats hight/low below the threshold. I would like to know. Thank you.
Hello,
For AC inputs a full bridge rectifier is used as shown in the below datasheet graphic.

When the AC input is on, the input will drive the rectifier on both the positive and negative cycle of the AC wave. The signal will be DC after the rectifier. Any ripple after rectification can be ignored since improper signaling will be prevented by the voltage thresholds.
The input thresholds are set by Rtht and Rsense. Please see section 9.2.1.2.4 - "Designing for Input Voltages Greater Than 60 V" - and How to Design Isolated Comparators for ±48V, 110V and 240V DC and AC Detection (Rev. A) for more details.
Best,
Andrew


As shown in the figure, even when the AC waveform is on, the output of "ISO1212" will repeat on and off.
If you do so, the output of "ISO1212" will be turned off even when it is normally turned on.
Is there no other way than to lower the threshold and reduce the off time?
What kind of measures do you usually take?
Thank you for your reply.
Hello,
Thank you for the diagram and clarification of the question. I understand that you are concerned about the output flickering as the rectified AC signals drops low. The Capacitor Cin should be sized large enough to smooth the ripple to a desirable level that will not cross the input thresholds set by Rthr and Rsense.

I hope this helps.
Best,
Andrew

The above is a reference circuit provided by TI. The capacitor value is 1nF. If you run a simulation with this value, the ripple will hardly disappear and it will be in an OFF state. Isn't the reference material recommended? Are there any recommended capacitor values? Thank you for your consideration.