This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6520: Using dual-channel isolator as a single channel isolator

Part Number: ISO6520

Hi TI,

Is it possible to use the dual-channel isolator ISO6520 as a single-channel device? 

If yes, how should I connect the unused input and output pins? 

I'm thinking about shorting the unused input to GND1 and shorting the unused output pin to GND2. 

Would this work okay? Or should I leave those unused pins open?