Part Number: ISOW1044
Other Parts Discussed in Thread: ISO1042
Tool/software:
Customer is worried about if different CAN transceivers on the same bus that could have conflict. For example, if the ISOW1044, ISO1042 and SN65HVD3082 are used on the same bus, what parameter we should take care and pay attention on.
As i know in general below are most care about with standard designs, what else and why? The most important i'd like to know is that behavior deviations between different part number.
- Termination method
- longer cables
- longer stub lengths
- number of nodes
- Input impedance of the CAN
Application: 5KVA UPS Module in the power rank.
Distance : <5 meter
Data Speed: <1Mbps
Regards
Brian