Part Number: ISOW7742
Tool/software:
Hi ISO team,
My customer has below question, could you comment on this.
I have a (very specific) question regarding the ISOW7742. The datasheet recommends usage of 330 ohm Ferrite Beads in the supply rails (and GND) on the non-isolated side. In the EVM and its documentation these are replaced with 1500 ohm Ferrite Beads. Both documents use 330 ohm Ferrite Beads on the isolated side. The difference on the non-isolated side makes me curious. Is the higher value the recommended one? Should we also go for this value? This could dampen EMC emissions. Is there a danger of ringing?
Another difference between the datasheet and the documentation of the EVM is that VIO and VISOIN use 0.1 µF instead of 0.01µF capacitors. Is that for stability or for EMC reasons?