This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6763-Q1: carrier frequencies

Part Number: ISO6763-Q1
Other Parts Discussed in Thread: ISO7763-Q1,

Tool/software:

Dear team,

Are the internal carrier frequencies of ISO7763-Q1 and ISO6763-Q1 same? What are the carrier frequencies?

Thank you!

  • Hello,

    Thank you for your question.

    The OOK carrier frequency of both ISO7763-Q1 and IDO6763-Q1 is around 450MHz and is used to modulate input signals and transmit them across the isolation barrier.

    Regards,
    Aaditya Vittal