Part Number: SN6507
Tool/software:
Hi team,
My customer tested short circuit on SN6507 EVM in room temp. It found IC temp can be up to 120 degrees during short circuit. Is this normal behavior? measure the SS pin voltage and found it's ~1.3V and then becomes 0 when short circuit happens.

In addition, how to understand "voltage dip is lower than 2.5 V"? does it mean voltage drop (Vt2 - Vt1 < 2.5V) lower than 2.5V? Because when there has no short circuit condition, the SS pin voltage is always 1.3V.

thanks a lot.
Best regards,
Yang