This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7841: ISOW7841FDWER digital isolator

Part Number: ISOW7841


Tool/software:

Dear team,

We are using the part number ISOW7841FDWER for digital isolator in BMS.

On primary side the 3.3v is connected through Power management IC(low voltage(LV)-12v I/P) and on secondary side the BMIC(battery monitoring IC ) is connected(high voltage(HV)-60v I/P).

the isolation barrier is their for the primary and secondary sections for digital isolator IC and communicated  through SPI interface i.e the BMIC is on secondary side connected through SPI to LV.

case1:-

When LV IS ON/ OFF the CS on secondary is pulled high and VREG FOR BMIC IC is not getting OFF.

When digital isolator is removed from board, the CS on secondary is pulled high and VREG FOR BMIC IC is getting OFF.

So the intended functionality is when LV goes off the digital isolator should go off and does have any enabled condition for CS and BMIC IC vreg should go off.

Will digital isolator cause any powering to the secondary load because of capacitive coupling and cause vreg to observe 5v as( CS pin is even pulled high)?

Best regards,

Navya.d

  • Hi Navya,

    Thank you for reaching out.

    I am not sure if I understand the problem statement correctly. Please share a schematic showing ISOW7841, VREG and the connections between. Please also explain understand what test conditions do you see the problem and also mention if VCC and VISO were powered under those conditions. Thanks.


    Regards,
    Koteshwar Rao