Part Number: ISOW1412
Tool/software:
I am working on a RS485 application with the ISOW1412. I have other communications that need to happen over the serial bus, but I am having trouble getting those to work properly when connected to the D and R outputs. I have RE/DE shorted to GND. Based on tables 10-2 and 10-3, I see that this will mean the ISOW1412 is driving R high, thus blocking any communications on that line, and that even with the EN/FLT pin pulled low this will still be the case. From this table I assume that in order to be able to have other devices use this line, RE will have to be pulled high.
However, for the line connected to D, I am also unable to drive signals on that line which I have not yet found behavior on the datasheet to explain. I tried grounding EN/FLT, which did not work (and based on the heat produced I'm guessing this is not intended operation). When I have D connected to the bus, I am unable to communicate with another serial device. I attached scope traces showing that when D is connected, the other device is unable to pull that line low, but when I disconnect D it works normally (see the amplitude differences between the two traces).
Any design insights would be much appreciated. Hopefully I am missing something obvious!
Thank you
-Nathan