Tool/software:
Hello Team TI
I need to know the impedance range of the component
PN: LFMDTBI-310-01004M
DESCRIPTION: IC BI31001004 XCVR CAN ISOLATED 16SOIC
MPN: ISO1050DWR
Since when consulting the spec of the technical sheet we do not see an impedance range reflected in K ohms
The serious question :
What impedance range can we have when measuring the tip of pins 12 CANL and 13 CANH on the component, this is due to the following.
We are having failures with materials that have an impedance range of 45 k ohms to 49 K ohms, materials with this range are failing us.
When doing an ABA test, we observed that the component that has a range of 50 k ohms to 55 k ohms is passing the tests correctly.
However, we do not know if the component can have an oscillation of minimum and maximum ranges.