Tool/software:
Hello,
What product corresponds to the PS2801C-1?
Additionally, in the cross-reference, the ISOM8110DFG is displayed as a drop-in replacement, but it seems that the pin pitch does not match.
Best regards,
DDdoor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
What product corresponds to the PS2801C-1?
Additionally, in the cross-reference, the ISOM8110DFG is displayed as a drop-in replacement, but it seems that the pin pitch does not match.
Best regards,
DDdoor
The PS2801C-1 has a CTR between 50 % and 400 %; the ISOM8110 and ISM8111 are inside this range. (There are no exact matches for the narrower CTR ranks, but in most circuits, you can use an ISOM811x device with a higher CTR).
The pin pitch indeed does not match. As far as I can see, the DFG package would be a replacement for the PS2501.
Hello DDoor,
ISOM8110 corresponds most closely to PS2801C-1. As Clemens mentioned the package does not match. Also, ISOM8110 has a much tighter CTR range and will generally stay around the 120% typical value over temperature and lifetime which eliminates the need for overdesign that is required with normal opto-emulators.
Best,
Andrew
Hello DDoor,
The key here is that an optocoupler with a high CTR is only advantageous if it is around its rated value with little variance. A optocoupler may have an extremely wide CTR range of 30% - 600% where the typical CTR is spec'd around 120%. This means that over lifetime, forward current and temperature the CTR can change dramatically and force the engineer to overdesign to compensate for the variation. This is why TI's opto-emulators are designed to have tight CTR ranges with little variance over lifetime and temperature. The opto-emulators are releasing in the CTR ranges shown below.

Best,
Andrew