Part Number: ISO1044
Other Parts Discussed in Thread: ISO6721
Tool/software:
The TCAN1044 DS says it can operate at 8Mbps. I realize this is beyond the ISO CAN specifications. My customer has asked about an isolated CAN device that can do 8Mbps. Is it possible that the ISO1044 can do 8Mbps, the same as the TCAN1044? I've been told that operating at 8Mbps is difficult because of the potential for the external circuitry to be a limitation. If my customer decides to try this, it would be at their risk to make sure all of the other challenges outside of the transceiver were solved. Thoughts?
Thanks,
Mark