Other Parts Discussed in Thread: ISO6721
Tool/software:
HI team,
I have a project and plan to use the ISO6721 for isolated UART communication.
When system is low power mode there is no communication through ISO6721. The Low voltage LV side supply is off, which means the VCC1 on the ISO6721 is completely off.
However the high voltage HV side supply is still on, which means 5V supply still apply on the VCC2.
The ICC1 will be 0A, but I am wondering is there any current on the ICC2? And if yes, what would this current be?
Thanks