Part Number: ISO1044
Tool/software:
Dear Experts,
We use ISO1044 in isolated application but in one case we do not need isolation for CAN but since we use
ISO1044 everywhere we do not want to introduce a new CAN transceiver so my question is is it possible to
use ISO1044 without isolation meaning that GND1 and GND2 are the same ground and VCC1 is driver by
the microcontroller's +3.3V supply, VCC2 instead is driver by the CAN bus +5V supply?
Thanks,
Andras