Part Number: ISO3082
Tool/software:
We use ISO3082DWR in our new project.
Symptom: We send the waveforms on the left of the following picture to RS485 A and B through the computer, and the feedback from RS485 A and B is like the waveforms on the right of the following picture.
Problem: The RS485 feedback waveform has less negative edges, and the amplitude of the waveform is reduced a lot. Help analyze what caused the problem,thanks.

The circuit design is as follows: R101 120Ω was removed , the R100 and R104 were changed to 0Ω, and the R97 and R105 pull-down resistors were removed during the test.