Part Number: ISOM8110
Tool/software:
Hi E2E Team,
do you have information for ISOM8110DFGRQ1 about the limits over temperature, because max. value is only specified for Ta = 25 °C?

Why are there no min / max values available?
Regards, Christian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOM8110
Tool/software:
Hi E2E Team,
do you have information for ISOM8110DFGRQ1 about the limits over temperature, because max. value is only specified for Ta = 25 °C?

Why are there no min / max values available?
Regards, Christian
Hello Christian,
Thank you for reaching out. The ISOM8110 does not have a cross-temperature min / max values for the timing specs. This because the specs would have too many dependencies on test setup and the device would have different responses over process voltage and temperature. It is common to represent the data as shown in the ISOM8110 datasheet. The timing characteristics are represented as a maximum for specific test conditions and the variance over temperature for a test condition is shown in the typical application curves.
I hope this helps.
Best,
Andrew