This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Internal Surge Protection is functional only in sink mode. The internal ESD structures can take current up to 1A and Voltage clamp at around 42V. Hence, if RTHR is surge proof resistor then surge protection is achieved without any additional Protection Components.
The ISO1228’s internal surge protection circuitry will pass surge tests if VSURGE / RTHR < 1A. External surge protection devices are needed if the peak surge current is in excess of 1A in one channel at a time. A common TVS diode used is TVS3300.