Part Number: ISO1228
Tool/software:
HI Sir
Due to space issue, we need to remove the led & Resistor replace it
have any issue?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1228
Tool/software:
HI Sir
Due to space issue, we need to remove the led & Resistor replace it
have any issue?

Hello Alex,
In order to maintain the wire break feature of the ISO1228, you can choose to use a diode if an LED is not needed. The device needs some consistent voltage drop for the wire detect feature to work. A resistor cannot be used because it will not have constant voltage drop. Any diode of voltage higher than 0.8V can be used for wire break.
Also, please review "Figure 8-2. Sinking Type Digital Inputs with ISO1228". The cathode of the diode/LED should be connected to AVSS and not in parallel with the input signal.
Best,
Andrew
Hello Alex,
The IN4148 should work to replace the LED since it has VF = 1V (assuming IF=100mA). Please let me know the updated schematic.
Best,
Andrew
Hi Alex,
The diodes are typically needed for full operation of the device. Certain features may be unavailable, however let me check with the team to see if there is a way to operate with less diodes or no diodes.
Hello Alex,
ISO1228 can operate without LED/diode in both sink and source mode but the wire break detection will not be available. “The LEDx pins can be connected directly to GND in sink mode provided wire-break detection is not used and V24V in source mode.” (7.3.2 Field Side LED Indication).
Best,
Andrew
hi Andrew
could you describe it detail? thanks
The LEDx pins can be connected directly to GND in sink mode provided wire-break detection is not used and V24V in source mode.” (7.3.2 Field Side LED Indication)
the pin is mean The LED

Hi Alex,
Good questions. Please allow me some extra time to answer them. I am checking with the team on a few items.
Best,
Andrew
Hello Alex,
You can use the size needed for your application. However, please keep in mind that the smaller resistors will need to be rated for the correct surge and power rating that your application requires.
Best,
Andrew
Hello Alex,
Thank you for your patience. To answer your questions, see below:
Best,
Andrew