Other Parts Discussed in Thread: TCA9517A,
Tool/software:
Hi Expert,
This is Shenzhen FAE Evan. My customer use TCA9517A as a buffer between system SOC I2C port and external HDMI I2C port as shown in the schematic below. And A side is connected to external HDMI port, B side is connected to internal system SOC I2C. The issue is that, one test item of HDMI certification is the port input capacitance(should be below 50pF@100kHz I2C signal). Now they want to change TCA9517A to ISO1640. The input capacitance Cio of ISO1640 can be found in datasheet 1pF, I need to confirm whether ISO1640 can keep the input capacitance free of the influence of system side circuit?