Part Number: SN6507
Tool/software:
Good day,
I seem to be missing a piece of information over and over while going through the datasheet.
How can the default voltage on the SS/ILIM pin be estimated?
The bias current on this pin is 275 uA typ. according to the datasheet, but the abolute maximum voltage on the pin must not exceed 6V.
Using the bias current (neglecting the leakage current) and an example R_ILIM = 47kΩ I get a voltage of 13V.
Is it internally capped at a certain voltage?
Furthermore, in section 8.3.6.2 "Over Current and Short Circuit Protection (OCP)" below the table 8-3 the following is stated:
"In the event of a transient overload or short circuit, if the resulting voltage dip is lower than 2.5 V (typical) on the SS/ILIM pin, the device considers it as a “soft-short” condition."
It's nowhere mentioned how the voltage behaves in relation to the input voltage/current through the switches.
Why should the voltage on the pin drop and why is the limit of 2.5V not mentioned anywhere else?
I am particularly interested in this in order to be able to select a capacitor with the appropriate DC bias.
If you could clear some things up for me, I would be very grateful!
Thanks in advance and best greetings,
Lukas Rettenbacher.