This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6501: SN6501 related issues

Part Number: SN6501

Tool/software:

Hello,

The schematic diagram of SN6501 is shown below. When the load is unloaded, the customer tests that the TP9 voltage is 4.3V. Under a 100 ohm resistor load, the TP9 voltage will drop to 4.1V. The LDO TPS76933 outputs 3.3V, which does not meet the LDO's VIN=VOUT+1V specification. Is there any application risk in this situation? How much current does an increase in load lead to LDO output not reaching 3.3V? Do you need to adjust the output of the transformer?

Thanks!