Part Number: ISO1044
Other Parts Discussed in Thread: ISO7721, , AM3352
Tool/software:
Hi,
We are using CAN communication as the system bus communication, and we are currently looking for a CAN device. We have an AM335x mounted on a custom board.
The DCAN module of the AM335x is equipped with CANH and CANL terminals, so CAN communication is possible without the intervention of any special device.
In addition, since the unit equipped with the AM335x may be inserted and removed, we are considering isolating the CAN communication.
As far as TI's isolated CAN transceiver is concerned, the connection on the controller side is made between the RXD and TCD terminals, so it cannot be connected to the CAN terminal of the AM335X.
Ideally, we are looking for a device like an isolated CAN repeater, but are there any products that you can suggest with a structure like CAN<--isolated-->CAN?
Are digital isolators such as ISO7721 applicable? Please tell us the recommended product model number.
Thanks,
Conor