Part Number: ISO3088
Other Parts Discussed in Thread: ESDS552, LMR16030, TSD05C
Tool/software:
HI Dan kisling
i have a question for you.
As you said adding one more TVS to the line will helps to conduct the High current surge( considering 1KV 42Ohm/ 23A since SM712 has 19A(8/20uA)).is it good to have varistor instead which capable of withstand 23A or more?
also i can see Line to line and line to GND in surge test procedures should we need a varistor across A to B, A to GND and B GND?

in a above picture they saying Earth reference is that Earth or Local GND (GND2 for the case ISO3088)