Part Number: ISOUSB211
Tool/software:
I hear a whine, whistle or hum in my audio application. Does TI have a device that can isolate the USB port and remove noise?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOUSB211
Tool/software:
I hear a whine, whistle or hum in my audio application. Does TI have a device that can isolate the USB port and remove noise?

Many applications have multiple paths to ground across the system. However, these ground paths can be the source of interference. The interference (called ground loop interference or a ground loop) is created when two or more devices in the same circuit have different ground potentials with respect to one another. Ground loop interference and shifting grounds can cause a variety of issues such as errors in data transmission or signal loss. The interference can even create a risk of electrical shock that can be hazardous to people or damage equipment in high-voltage applications.
Audio applications are particularly susceptible to small interferences in the audible range that can be caused by low-cost and unbalanced power solutions in computers and interfaces. TI's Isolation solutions feature best in class-isolation that can be used to remove these ground loops. For more information, please see USB Audio Isolation with Isolated USB 2.0 Redriver.