Part Number: ISO1212
Tool/software:
Hi,
On a new design I used the ISO1212 for DI. I copied the reference design as shown below:

Rthr is 1k and Rsens is 562 Ohm
I measure a current of about 20mA as soon as I apply 24V on the Rthr input. The device output is not switching and stays at 0V. The Voltage on the Sense Pin is 7V therefore we have about 17mA of current inside RTHR. (24-7)/1k
Any suggestion why my ISO1212 needs that much current?
I also measured a second PCB with the same result.
Thanks for your answers!
Cheers,
Chris