Other Parts Discussed in Thread: SN6505A-Q1, SN6505A, SN6505B, SN6505D
Tool/software:
Hello,
I would like to use SN6505B-Q1 for isolating power for ECG use. I would like to know:
1. What is the difference between SN6505A-Q1 SN6505B-Q1 or SN6505BDQ1 except for the minimal frequency ?
2. In the datasheet there was a table with " Recommended Isolation Transformers Optimized for the Device". Is it must using only them with the device ? If I found conditions are met with other transformer isn't it possible to use it ?
For example: 76253/35ENC of MURATA with 1:2.23CT is not OK to use with that driver?
Thanks,
Ohad