Tool/software:
The absolute max allows 3.3V for the CAN bus side but the recommended operating conditions state 4.5-5.5V. Has the part been qualified, perhaps limited to1MHz, at 3.3V or another lower CAN bus side supply voltage?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The absolute max allows 3.3V for the CAN bus side but the recommended operating conditions state 4.5-5.5V. Has the part been qualified, perhaps limited to1MHz, at 3.3V or another lower CAN bus side supply voltage?
Hello Bob,
Thank you for reaching out. The device has not been qualified for derated performance outside of the recommended operating conditions. Datasheet performance specs are only guaranteed within the recommended operating conditions. Therefore, the VCC2 recommended range of 4.5-5.5V need to be met for datasheet CAN performance.
Best,
Andrew