This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7320-Q1: How to understand the Viowm of isolator

Part Number: ISO7320-Q1
Other Parts Discussed in Thread: ISO7720-Q1,

Tool/software:

Hi

I'd like to use an isolator for CAN signal isolation in HEV automotive applications.

There is a parameter which named Viowm in spec of ISO7320.

How should I understand the Viowm. It shows 400Vrms.

Does that mean I can't use it in the 800V car system?

Regards

Arrow