Tool/software:
Hello,
We are using ISO1450 for Half-Dublex communication with RS422.
In our application ISO1450 only receives RS422 signal from rs232 to rs422 converter. The converter is connected to the sensor. But there was a problem to receive. The issue is when we try to connect converter to the ISO1450, voltage level on the B pin side is drops.
The oscilloscope images are:
Without ISO1450 connection:
With ISO1450 connection.
I need to mention that we enable both Receive Enable and Drive Enable pins.