Part Number: ISO7340-Q1
Other Parts Discussed in Thread: TMS320F28379D
Tool/software:
Dear TI team,
I have a few questions regarding the working and failure conditions of the ISO7340-Q1 high state isolator. The supply voltages are Vcc1 at 3.3V and Vcc2 at 5.3V. The Vcc1 digital pins are connected to the TMS320F28379D GPIO pins, while the Vcc2 digital pins are connected to the Cryton MD20A board.
If I apply 2.5V to pin 13 and 0.75V to pin 11 while maintaining 3.3V at pins 4 and 6 (which are input pins), what effects can I expect?
Similarly, if I apply 2.5V to pin 13 and 0.75V to pin 11 while pin 4 and pin 6 are at 0V, what will be the outcome?
attached images for your reference


Thank you for your assistance!