Part Number: ISO1050
Other Parts Discussed in Thread: ISO1042, ISO1044
Tool/software:
Hi TI Team,
Our customer required CAN communication with minimal baud rate of 10kbps.
Accordingly the datasheet it is possible.
SLLS983L – JUNE 2009 – REVISED OCTOBER 2023
Dominant time out, tTXD_DTO – min 1,2ms
Minimum Data Rate = 11 / tTXD_DTO -> 9,2kbps
But our test shows an error.
It looks like we are using an old revision of the IC.
SLLS983J –JUNE 2009–REVISED SEPTEMBER 2019
Dominant time out, tTXD_DTO – min 300us
Minimum Data Rate = 11 / tTXD_DTO -> 37kbps
Unfortunately, both data sheets have the same ordering code - ISO1050DWR.
Please provide us with the complete order code for the current revision of ISO1050.
Thanks.
Regards, Dmitri