Other Parts Discussed in Thread: ISO1050, SN6501
Tool/software:
Hello Here,
This is Racheal from Shenzhen site AA3 team. My customer InfyPower wants to use ISOW7842 in their products. Here is the application info:
ISOW7842 selection reason: update from ISO1050, with DCDC integrated inside ISOW7842, aux-power simplified.
Input VDD: 3.3V
signal chain: DSP – Isolation – CAN transceiver(NON-ISO)
Output current: 100mA.
Output VDD: 5V
The datasheet indicates the device capable of outputting over 40mA. But this still cannot meet the customer’s need. So we’d like to know what’s the exact limit?
Because the customer believes that this device cannot output 100mA, he selects NSIP8842 as isolation device, which applies 3.3V_VIO and 5V_VDD in the primary side separately. If ISOW7842 is not suitable to the application scenario, could you recommend other solutions?
Thanks,
Racheal Shen