Other Parts Discussed in Thread: ISO1432,
Tool/software:
Hello,
I checked both ISO1432 and ISOW1412. Both seems to meet my specifications but I really liked that the ISOW1412 has the isolated DCDC built-in.
I want to send a RS-485 communication through a 2 meter cable. My idea is to put an ISOW1412 on the control board and a ISO1432 on the daughter board.
Do I need that both transceivers are powered locally on their secondary side? Could I send the power generated by the ISOW1412 through the cable so it powers up the secondary side of the ISO1432?
Regarding shielding the cable, should I connect the shield to the isolated GND of both transceivers?
Thank you