Part Number: SN6507
Other Parts Discussed in Thread: POWERSTAGE-DESIGNER
Tool/software:
Customer would like to do the bias power of gate driver for AC inverter. Is there ref. design similar to below condition?
Input Voltage: 24V+/-5%
Isolated Output Voltage: 24V (x3)
Remark: There're three 24V ISO outputs for IGBT's bias power. The total output power is about 5W. Could SN6507 using only one transformer to do so? thanks.
Regards
Brian