Other Parts Discussed in Thread: ISO1410
Tool/software:
Hello, I would like to understand the input requirements of the ISO3088 A little better. Figure 6-10 shows minimum recommended Differential Input Voltage vs Signal Rate. I am running at 10Mbps so it recommends a differential voltage of about 650mV.

Say I have a square wave as the input signal. Does graph 6-10 mean the voltage from the top of my square wave to the base of my square wave should be 650mV total swing or does it require +650mV to -650mV. I have seen the definitions of Vid in Figure 7-7. There is no accompanying waveform so I am unclear.
If the input hysteresis thresholds are all between -200mV and -10mV (Table 6.9), why does Fig 6-10 recommend a 600mV swing all the way down to DC? The A/B input schematics in 8.4.1 don't look to me like a traditional differential amplifer (unless that emitter current source is shared between the inputs). Is it possible to share a more detailed schematic of the differential input section?