Tool/software:
Is it possible to get say something about the construction and material requirements of the ISOW14x2 for reinforced insulation according to DIN VDE V 0884-11 or IEC 60747-17?
Thank you in advance,
Håkon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Is it possible to get say something about the construction and material requirements of the ISOW14x2 for reinforced insulation according to DIN VDE V 0884-11 or IEC 60747-17?
Thank you in advance,
Håkon
Hi Hakon,
Thank you for your interest in ISOW1432.
If you are asking whether DIN VDE V 0884-11 or IEC 60747-17 have any requirements to use a specific construction and material, then the answer is no. I do not believe they require us to use a specific construction or material but they do consider specific margins certifying isolation ratings. I am copying below the screenshot from datasheet which describes the margins considered by VDE in granting isolation ratings.

If you meant to understand more about the construction and material of ISOW1432 isolation barrier (capacitor), then the following links provide you the details in this regard. Let me know if you have any further questions, thanks.
Regards,
Koteshwar Rao