Part Number: ISO1042-Q1
Other Parts Discussed in Thread: ISOM8610
Tool/software:
Hi Experts,
Seeking your assistance on this query using ISO1042QDWRQ1 for CAN interface. It is terminated by a 120 ohm resistance using 2 OptoMOS switches:
When CAN output is ON and 120 ohm termination resistance is checked between CAN_H and CAN_L, the resistance keeps on varying. Continuously between 500 ohm and 30 ohm. Fluctuating random values. When CAN output is turned OFF, the resistance can be measured as 122 ohms. Why is resistance changing when CAN data is ON?
Thank you.
Regards,
Archie A.