This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC15241-Q1: efficiency at 2.5W input power

Part Number: UCC15241-Q1


Tool/software:

Hi,
which load could a UCC15241 deliver with a supply from an other UCC15241. (Two of them in series)
The first UCC15241 will deliver 2.5W at 24V output. I will use this as supply for the second one.
To get a bigger isolation distance.

Is a diagram available with efficiency over output current?

Regards Reiner