Tool/software:
Hi,
I am using ISO7741FBDWR as isolated 1mbps UART. I found that communication is not being transferred to isolated side from MCU.I am attaching my schematics> Please let me know if there is any mistake
Thanks & Regards
Mounish
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I am using ISO7741FBDWR as isolated 1mbps UART. I found that communication is not being transferred to isolated side from MCU.I am attaching my schematics> Please let me know if there is any mistake
Thanks & Regards
Mounish
The schematic does not show decoupling capacitors.
The IN pins are inputs, the OUT pins are outputs. As far as I can see, the MCU_TX signal should go through channel D.
The idle state of UART signals is high; you should use the isolator without the F suffix.
Hi Mounish,
As Clemens stated, there are no decoupling capacitors of 0.1uF present on the VCC pins. We highly recommend these decoupling capacitors as they allow for proper functionality of the device.
Also, I see that the "F" version of the device is used meaning that the default state is LOW. As Clemens mentioned, the non-F version may be more beneficial for you since the idle UART signal state is HIGH.
Please Also review the signal Input and outputs. This may be a mistake in the schematic diagram itself but the MCU_TX signal is pointing inwards, so I am not sure if that means it is an input to the isolator or an output that is going to the MCU.
Regards,
Aaditya Vittal