Tool/software:
Hello?
I would suggest the additional fabrication of isolated signal transmission components in space-grade products.
Currently, the only space-grade product is the ISOS141FDBQSEP with 3/1 ch, but I would like to use the 4/0 ch and 6/0 ch as well.
Below EM, commercial grade -> Above EM, space grade
ISO7741FDBQ -> ISOS141FDBQSEP (for isolated SPI communication)
ISO7740FDBQ -> like ISOS140FDBQSEP? (for isolated single-phase full-bridge with bootstrap)
ISO7760FDBQ -> like ISOS160FDBQSEP? (for isolated three-phase full-bridge with bootstrap)
Currently, I'm planning to deploy more ISOS141, but if there is a new product, I think the burden due to space constraints will be reduced. (especially 6/0 ch)
S.Y.Lee