This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7231M: DW's RΘJA is

Part Number: ISO7231M


Tool/software:

Hi, Staff

Please let me check the specifications of ISO7231M (SLLS867L).

6.3 Thermal Information states that RΘJA is 168℃/W for the DW-package.
However, in the TEST CONDITIONS of 6.8 Safety Limiting Values, RΘJA is presented as 212℃/W.

・Which is the correct RΘJA for DW: 168℃/W or 212℃/W?
・If I modify a datasheet, will a new PCN be issued?

regards
cafain