Part Number: ISOUSB211
Tool/software:
I've been working on a device that uses the ISOUSB211 IC for USB data isolation. The throughput is relatively high, around 300Mbps, and we are failing our radiated emissions at 225MHz. Our testing shows that when there are a high number of signal transitions on the USB line, we see very defined spikes at multiples of 7.5MHz (the spectrum analyzer settings didn't allow me to put the marker on 67.5MHz exactly there, so ignore that value).
Does the chip have an internal clock of 7.5MHz or 15MHz? Any tips on reducing the radiated emissions at these frequencies?
Thanks!
The following is a spectrum analyzer shot of this using a loop antenna. We also did conducted emissions measurements on the USB pins of the isolator and we see these frequencies on both sides.