Tool/software:
e2e,
Could you comment on the storage time (ts) parameter. There is no comment on what it is other than Figure 7-3 showing that it is part of toff. Section 6.8 shows a maximum of 21us which is much slower than the worst-case toff of 14.5us.

When I look at Figure 6-29, I see a ts of about 6.1us. That graph is for Rl-4.7K, If = 1.6mA and Vcc = 5V which is the same setup for the ts spec of 21us.
I previously was told the spec was characterized at room temperature according to the datasheet. For variance overtemperature you can use Figure 7-11. Switching Time vs Ambient Temperature to find the results specific to your use case. Part to part variances on timing spec is +/- 20%, but most devices will be around the typical value.” But 21us is a lot more than +20% of any toff times listed for this part.
Just trying to understand what I’m missing.
Adam