Part Number: ISO1228
Other Parts Discussed in Thread: ISO7741, ISOM8710, ISO1212, , ISO7740, ISO7741EVM
Tool/software:
I am using three AC/DC programmable power supplies (HDS3000-12) in parallel for my application. Each power supply provides a "POWER OK" (POK) signal, which is connected to the PLC digital input module (AXL SE DI16/1 NPN). However, due to differences in grounding, I am unable to reliably detect feedback signals (True/False).
I believe that a digital signal isolator is necessary to address the grounding issue while maintaining electrical isolation. Could you provide advice or suggest a suitable circuit design for this purpose? You can also suggest any other option or IC that can be usable.
1. PLC Di module AXL SE DI16/1 NPN - Digital module

2. Power Supply HDS3000-12