Other Parts Discussed in Thread: ISO7741, ISO1042
Tool/software:
Hi Expert,
Could you help to recommend one device could be transmit SPI to CAN protocol, also integrated isolation function. thanks.
BR
Chi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Chi,
Thank you for reaching out. ISO1042 is an isolated CAN transceiver that can take be used to isolate and interface with the CAN bus. ISO7741 can be used to isolate the SPI signals. However, we do not have an isolated SPI to CAN device, and you will need something to convert the between the protocols.
Best,
Andrew