Part Number: ISOW7741
Other Parts Discussed in Thread: ISO6441, LM5181, ISOW7841
Tool/software:
Hey Isolation Team,
I have a customer evaluating the ISOW7741 for a new project and it will be used in an application that will only be drawing around 5mA of load current through the device. Based on the efficiency graph (Figure 7-6 in the device DS) it looks like there is quite a steep drop-off in efficiency at load currents below 20mA.
Can this device tolerate and operate at loads around 5mA? Is there another device in your portfolio similar to the ISOW7741 that would be better suited for these lower load currents?
Best regards,
Matt Calvo