Part Number: ISO1450
Tool/software:
Hi Team,
Our customer is considering replacing their NVE IL485E with an ISO1450DW and would like to know if there are any concerns regarding this.
Reason for device selection
In a field environment where the communication idle time potential is about 30mV,
IL485E
Positive input threshold voltage max: 200mV
Negative input threshold voltage min: -200mV
In this environment, it is in an undefined range and communication is not possible.
In contrast,
ISO1450DW
Positive input threshold voltage max: -10mV
Negative input threshold voltage min: -200mV
By putting the communication idle time potential outside the undefined range, communication is improved, so this device was selected.
Terminal 10 of the IL485E is not used, so there are no problems with functionality.
Could you please let me know if you have any other concerns regarding this replacement?
Best regards,