Part Number: SN6505B
Tool/software:
Hi team,
Our customer performed ESD test with this device, and observed switching stoped momentarity.
We guess this is because this device is disabled by EN pin or UVLO enable.
Please tell us about below question,
1. In datasheet 8.2 Block diagram, UVLO block is connected EN pin, but Table 5-1 says that UVLO is in Vcc description and the threshold is decides by Vcc voltage.
Is this correct that UVLO is detected at Vcc pin?
2. How mach are there delay of device enable by EN pin and delay of UVLO enable after detected?
3. In this datasheet 8.4.5 External Clock Mode, it is said that "The device also has external clock fail safe feature which automatically switches the device to the internal clock if a valid input clock is not present for long (tCLKTIMER).". How does this device detect valid external clock?
4. EN pin and CLK pin is pulled-down by internal resister. How much is both of the resistance value?
5. In datasheet 8.2 Block diagram, there are two GND pin. Why is this?
Best regards,
teritama