Part Number: ISO6760
Tool/software:
We have received questions about the ISO676x series.
Kindly please answer two questions. Thanks.
ISO6760FDWR www.ti.com/.../iso6760.pdf
- The CMTI value has changed from current 130 to proposed 150 in the revision of Datasheet Ver C to D (Sections "6.9", "6.11" and "6.13") in May 2022.
We would like to know the reasons for these changes.
- The notation of product life span has changed in "Fig. 9-8".
The life spans have changed as follows. Please explain why they have become shorter.
Also, the x-axis of the graphs in datasheet Ver.D and later versions starts at 200. It is difficult to compare with previous versions. Could you please provide a graph where the x-axis starts at 500?
VDE Safety Margin Zone : 254Yrs to 54 Yrs
Operating Zone : 135Yrs to 36 Yrs
Junji,