This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6507: SN6507 Custom transformer design

Part Number: SN6507


Tool/software:

Hi,

I need to design a isolated DC/DC converter for 24V input, 5V@500mA output using SN6507. I would like to go with custom toroidal transformer design.

I have no difficulties to calculate the Vt product, transformer turns ratio and all other parameters and resistance values.

How to calculate the number of primary turns or primary inductance value with Vt product? Is ther any formula or application notes to do the calculations?

I'm using a senduct toroidal core KS050-125A and I have attached the datasheet of the core here. Please help me to calculate the number of primary turns or primary inductance of the transformer with the given core material.

Udhay

KS050-125A.pdf