Part Number: UCC15241-Q1
Tool/software:
Hello everyone,
I am working on a project where I need to use the UCC15241-Q1 to achieve an isolated 18V and 0V output from a 24V input. This isolated DC/DC module will be used with my SiC MOSFET. Could someone guide me on the appropriate resistor values to achieve a single 18V-0V output? I am referring to the following circuit diagram: